image

Slant 01, top banner

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Sit amet, consectetur adipiscing. Error sit voluptatem accusantium doloremque.

Learn More

image

Slant 01, bottom banner

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Sit amet, consectetur adipiscing.

Learn More

image

Slant 02, top banner

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Sit amet, consectetur adipiscing. Error sit voluptatem accusantium doloremque.

Slant 02, bottom banner

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Sit amet, consectetur adipiscing. Error sit voluptatem accusantium doloremque.

Fill out the form to register now

image

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Sit amet, consectetur adipiscing. Error sit voluptatem accusantium doloremque.

image

Lorem ipsum dolor sit amet, consectetur adipiscing elit. Sit amet, consectetur adipiscing. Error sit voluptatem accusantium doloremque.

banner image

Banner 01

Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod.
banner image

Banner 04

Lorem ipsum dolor sit amet, consectetur adipiscing elit, sed do eiusmod tempor incididunt ut labore et dolore magna aliqua. Ut enim ad minim veniam, quis nostrud exercitation.








The Importance of Cable Cleats within Data Center Electrical Systems

In the information age, data centers and their task of continuous, safe storage of data make them critical facilities. If the data center isn’t reliable, business can’t be done.

This webinar outlines the importance of the engineered cable cleat when considering power cable system design and installation in data centers. Panduit's experiences is drawn from almost 25 years of design, manufacture, business leadership, research and development of cable cleats, including hundreds of live short circuit tests.

Who should attend:
  • Contractors (for Data Centres)
  • Electrical Installers or Licensed Electrical Worker
  • Safety Engineers
  • Electrical Engineers
  • Data Centre Designer
  • Fire Safety Engineer
In this webinar, we will cover the following topic:
  • Power system protections and their regulations
  • Installation issues and failures
  • Importance of a correct specification of Cable Cleat
  • Challenge the standing perceptions 
  • Introduction to Panduit's award winning fault simulation software
  • Live Q&A session

Thank you for registering.

You will receive a confirmation email from Panduit Asia Pacific <customercare@gotowebinar.com> shortly with your unique webinar login for The Importance of Cable Cleats within Data Centre Electrical Systems on 06 May 2020 at 11:00AM to 12:00PM.


Share:

Please contact contactap@panduit.com if you do not receive your email within the next 24 hours.




Commonly Asked Questions about The Importance of Cable Cleats within Data Center Electrical Systems

  1. Do I need to think about corrosion with cable cleats?
    Panduit's stainless steel cable cleats (Trefoil, Locking Strap, Buckle Strap) are made of stainless steel 316L with strong anti-corrosion property. Corrosion will not be a concern even in extreme environments.

  2. Why does the market continue to specify cleats with force rating at 1s even though max force occurs at 0.04 or 0.05 secs?
    Whenever we see a 1s or 3s short circuit, it relates to the I²t of the cable (or switch gear). For cable, we refer to the amount of current that size conductor can take for that 1s or 3s period. This is a different short circuit requirement to the instantaneous forces during a phase to phase fault.

  3. Will this be part of inspections standards specially in certifying data center tier?
    It varies from project to project. More EPCs and Contractors are beginning to be aware of the importance of cleats in data centers. As such, they will need to know that specifying cleats that are compliant to IEC 61914:2015 is one of the first steps to protect their power systems. Going forward, inspections to ensure compliance will become a norm.

  4. Is there also a cable bundling standard practice for communication cable like copper UTP and fiber optic cable?
    There is no standard that specifically instructs on cable cleat installations. The NEC and The Cable Tray Institute provide guidelines for securing cable on horizontal and vertical runs, but cable cleat spacing is determined by the calculated forces during a short circuit fault.

  5. Can your cable cleat install in standard wire tray?
    Panduit has unique mounting brackets (eg. I-Beam, Top Hat and Round Type) that can help with the installation of cleat onto the cable tray. Check out our installation videos in the webpage.

  6. For a vertical cable installation, the cable cleat will also hold the cable weight. Is there a specification of each type of cable cleat and how much weight it can hold?
    IEC 61914:2015 requires an axial test to be performed to securely hold the cable in position. This test is carried out using the smallest cables in the range and at an elevated temperature. The vertical load is applied and held for 5 minutes. A maximum displacement of 5mm is allowed. All manufacturers should publish the axial / vertical performance on their data sheets.

  7. How was the ordering of cleats, is there a minimum quantity of ordering?
    You can order Panduit's cable cleats through your local distributors. The standard MOQ is 10 pieces / part number.

  8. Is this already available in the market?
    Yes, all Stainless Steel, Aluminum and Polymer cleats are available in the market.

  9. What is the max cables size the cleat can secure?
    SS Trefoil Clamp Style or CCSSTR - 69 mm; Buckle Strap Cleat (double loop) - 86 mm; Buckle Strap Cleat (trefoil Triple Loop) - 53 mm; Locking Strap Cleat (trefoil double loop) - 100 mm; Locking Strap Cleat (flat multicore double loop) - 195 mm. For cables with bigger OD sizes than the ones stated above, please approach your local Panduit distributor or Panduit Sales representative for more information.

  10. Do you have stainless steel cable clip for solar farm to hold (4 x 6) mmsq cable?
    Yes.

  11. Does it make sense to use cable cleat for outdoor type fiber cables in the vertical riser spaces? 
    Fiber cables unlike power cables will not experience short circuit faults. Hence cable cleats are not needed.

  12. We can still use cable tie instead of cable cleats . Why would customers agree to use it? What is the main benefit?
    If you continue to use cable ties instead of proper cable cleats, your power system and infrastructure will be at risk as the cable ties are unable to secure the power cables during a short circuit fault.

  13. Is this cable cleats only for electrical cable or can use for data cable also? For e.g: fiber optic cable?
    Cable cleats are for power electrical cables only.

  14. How about the warranty of the item? Is it lifetime warranty?
    We provide one-year standard Panduit limited warranty.


Why Cable Cleats are Vital to Protect Major Infrastructure Projects?

How Panduit can help to ensure your infrastructure projects will be completed safely, on time and under budget?


Strapping Bands vs. Cable Cleats – Exposing the Misconceptions

How Panduit challenges the misconceptions and offers a more logical, engineered route to the correct specification of a cable fixing system?


Two-thirds left content

Ut quis nostrud exerci tation ullamcorper adipiscing elit, sed diam nonummy nibh euismodtincidunt suscipit lobortis nisl ut aliquip ex ea commodo consequat. At vero eos et accusamus et iusto odio dignissimos ducimus qui blanditiis praesentium voluptatum deleniti atque corrupti quos dolores et quas molestias excepturi sint occaecati cupiditate non provident, similique sunt in culpa qui officia deserunt voluptatem quia voluptas sit aspernatur aut odit aut fugit, sed fuga.

Lorem ipsum dolor sit amet, consectetuer adipiscing elit, sed diam nonummy nibh euismod tincidunt ut laoreet dolore magna aliquam erat volutpat.

Ut quis nostrud exerci tation ullamcorper adipiscing elit, sed diam nonummy nibh euismodtincidunt suscipit lobortis nisl ut aliquip ex ea commodo consequat. At vero eos et accusamus et iusto odio dignissimos ducimus qui blanditiis praesentium voluptatum deleniti atque corrupti quos dolores et quas molestias excepturi sint occaecati cupiditate non provident, similique sunt in culpa qui officia deserunt voluptatem quia voluptas sit aspernatur aut odit aut fugit, sed fuga.

Lorem ipsum dolor sit amet, consectetuer adipiscing elit, sed diam nonummy nibh euismod tincidunt ut laoreet dolore magna aliquam erat volutpat.

Sed ut perspiciatis unde omnis iste natus error sit voluptatem accusantium doloremque laudantium, totam rem aperiam, eaque ipsa quae ab illo inventore veritatis et quasi architecto beatae vitae dicta sunt explicabo. Nemo enim ipsam voluptatem quia voluptas sit aspernatur aut odit aut fugit, sed quia.

Ut quis nostrud exerci tation ullamcorper adipiscing elit, sed diam nonummy nibh euismodtincidunt suscipit lobortis nisl ut aliquip ex ea commodo consequat. At vero eos et accusamus et iusto odio dignissimos ducimus qui blanditiis praesentium voluptatum deleniti atque corrupti quos dolores et quas molestias excepturi sint occaecati cupiditate non provident, similique sunt in culpa qui officia deserunt voluptatem quia voluptas sit aspernatur aut odit aut fugit, sed fuga.

Two-thirds right content

Ut quis nostrud exerci tation ullamcorper adipiscing elit, sed diam nonummy nibh euismodtincidunt suscipit lobortis nisl ut aliquip ex ea commodo consequat. At vero eos et accusamus et iusto odio dignissimos ducimus qui blanditiis praesentium voluptatum deleniti atque corrupti quos dolores et quas molestias excepturi sint occaecati cupiditate non provident, similique sunt in culpa qui officia deserunt voluptatem quia voluptas sit aspernatur aut odit aut fugit, sed fuga.

Sed ut perspiciatis unde omnis iste natus error sit voluptatem accusantium doloremque laudantium, totam rem aperiam, eaque ipsa quae ab illo inventore veritatis et quasi architecto beatae vitae dicta sunt explicabo. Nemo enim ipsam voluptatem quia voluptas sit aspernatur aut odit aut fugit, sed quia.

Lorem ipsum dolor sit amet, consectetuer adipiscing elit, sed diam nonummy nibh euismod tincidunt ut laoreet dolore magna aliquam erat volutpat.

Ut quis nostrud exerci tation ullamcorper adipiscing elit, sed diam nonummy nibh euismodtincidunt suscipit lobortis nisl ut aliquip ex ea commodo consequat. At vero eos et accusamus et iusto odio dignissimos ducimus qui blanditiis praesentium voluptatum deleniti atque corrupti quos dolores et quas molestias excepturi sint occaecati cupiditate non provident, similique sunt in culpa qui officia deserunt voluptatem quia voluptas sit aspernatur aut odit aut fugit, sed fuga.

Lorem ipsum dolor sit amet, consectetuer adipiscing elit, sed diam nonummy nibh euismod tincidunt ut laoreet dolore magna aliquam erat volutpat.

Ut quis nostrud exerci tation ullamcorper adipiscing elit, sed diam nonummy nibh euismodtincidunt suscipit lobortis nisl ut aliquip ex ea commodo consequat. At vero eos et accusamus et iusto odio dignissimos ducimus qui blanditiis praesentium voluptatum deleniti atque corrupti quos dolores et quas molestias excepturi sint occaecati cupiditate non provident, similique sunt in culpa qui officia deserunt voluptatem quia voluptas sit aspernatur aut odit aut fugit, sed fuga.

Sidebar left

Lorem ipsum dolor sit amet, consectetuer adipiscing elit, sed diam nonummy nibh euismod.

Lorem nibh euismod tincidunt ut laoreet dolore magna aliquam erat.

Sidebar left

At vero eos et accusamus et iusto odio dignissimos ducimus qui blanditiis praesentium voluptatum deleniti atque corrupti quos dolores et quas molestias excepturi sint occaecati cupiditate non provident, similique sunt in culpa qui officia deserunt voluptatem quia voluptas sit aspernatur aut odit aut fugit, sed fuga.

At vero eos et accusamus et iusto odio dignissimos ducimus qui blanditiis praesentium voluptatum deleniti atque corrupti quos dolores et quas molestias excepturi sint occaecati cupiditate non provident, similique sunt in culpa qui officia deserunt voluptatem quia voluptas sit aspernatur aut odit aut fugit, sed fuga.

Content video

Lorem ipsum dolor sit amet, consectetuer adipiscing elit, sed diam nonummy nibh euismod tincidunt ut laoreet dolore magna aliquam erat volutpat.

Video headline

Above video - Lorem ipsum dolor sit amet, consectetuer adipiscing elit, sed diam nonummy nibh euismod tincidunt ut laoreet dolore magna aliquam erat volutpat.

Below video - Lorem ipsum dolor sit amet, consectetuer adipiscing elit, sed diam nonummy nibh euismod tincidunt ut laoreet dolore magna aliquam erat volutpat.

Statistics

32%

Sed quia non numquam eius modi tempora incidunt

2/3

Autem vel eum iure reprehe nderit qui in ea voluptate

76%

Nam sit amet tellus non felis dapibus molestie lorem

Learn More

Get in touch with Panduit

To learn more about our global engineered custom solutions and technical support, talk to us now.

SUBMIT YOUR BUSINESS INQUIRY NOW!

Download Whitepapers

Asset Grid

Outcomes Grid

Reprehe nderit qui in ea voluptate reprehe nderit qui in ea voluptate reprehe nderit qui in ea voluptate reprehe nderit qui in ea voluptate.