LARGE PARAGRAPH TEXT FOR LONGER DESCRIPTIONS
The key features and benefits:
05/04/2023 - Panduit, a leading manufacturer of infrastructure solutions, has expanded its cable fastening series. The existing metal Solar Edge Clips can already be installed without tools in around 11 seconds - 10 seconds faster than average cable tie and clip combinations, a time saving of almost 50%. Panduit's new Edge Clips are versatile, quick, and secure to attach directly to panel and frame edges. This allows cables or wires to be routed along or perpendicular to the edge in a user-friendly manner. To do this, simply press the clip directly onto the respective edge and use the matching cable tie for bundling. Drilling into the existing structure is unnecessary, components remain intact to resist corrosion and overall installation efficiency is increased. The new Edge Clips offer more flexibility due to their wider range of use. The two variants are suitable for 0.7 to 3 mm and for 3 to 6 mm thick edges. In addition, you only need one Edge Clip for horizontal or vertical mounting, where normally two different Edge Clips are necessary. This reduces the space of storage required and gives you much more flexibility when mounting on site. Particularly clever: the specially designed saddle presses the cable tie firmly against the Edge Clip with no slippage. The compact mounts thus ensure a permanently firm, secure fit, even if you pull a cable through the fasteners. The high-performance clips offer high tensile strength thanks to the specially developed metal lips and can still be attached by hand without tools. The range of applications is enormous. The combination of innovative Edge Clips, robust cable ties and cable tie bases from Panduit find their professional use in the cabling of motor vehicles, rail vehicles, heavy-duty machinery, trucks, all the way to solar parks for cable routing underneath panels. In addition, Panduit offers pre-configured assemblies or barbed versions for applications with very high vibrations.
About Panduit
For more than 60 years, Panduit has been the world's leading provider of innovative solutions in the field of physical and electrical infrastructure for data centers, industrial and building automation and related services. Headquartered in Tinley Park, IL, USA, with offices in 112 locations worldwide, Panduit stands for quality and innovative technologies. The family-owned company with more than 5,000 qualified employees generates sales in the billion Euro range worldwide. Panduit owes its outstanding market position to the constant striving for innovation and the untiring commitment of its employees. The global player invests above average in research and development, in first-class production, in the best possible support of its sales channels and in excellent customer service. This, combined with a strong partner network, is the prerequisite for comprehensive support, sustainability, and solid corporate growth in the networked world of today and tomorrow.
Large Paragraph Text Used As A Subheading
Lorem ipsum dolor sit amet, consectetuer adipiscing elit, sed diam nonummy nibh laoreet volutpat.
— John Doe | Job Title, Company
Pellentesque non magna eget ex lobortis finibus. Lorem ipsum dolor sit amet, consectetur adipiscing elit. Etiam nec arcu non eros hendrerit viverra a vitae libero. Etiam et ultricies nulla. Donec euismod lectus magna, eu dignissim mauris hendrerit vulputate.
Pellentesque non magna eget ex lobortis finibus. Lorem ipsum dolor sit amet, consectetur adipiscing elit. Etiam nec arcu non eros hendrerit viverra a vitae libero. Etiam et ultricies nulla. Donec euismod lectus magna, eu dignissim mauris hendrerit vulputate.