Why You Should Trust AVTs Webinar
Q1: How many years or number of tests is the battery expected to last? Answer: The battery can last for 5 years under normal operating conditions. However, there are considerations like temperature extremes and the frequency of use which can affect the battery life. Once you push the test button and if the yellow caution indicator does not start flashing, you should replace the battery immediately.
Q2: What equipment can AVTs be used on, motor control centers or panels? Answer: AVT can be installed on any equipment under 600 volts that you would typically test for absence of voltage. Motor control centers, panels or switch gears, are the biggest applications that we' have seen so far but key use cases would be any equipment that you frequently enter or have high risk when you enter to access your panel.
Q3: Any suggestions on how to change the workplace culture? How do you convince an electrician to trust the VeriSafe AVT versus his usual handheld meter? Answer: Perform trial runs by installing a few VeriSafe units throughout the facility just to get the electricians and the operators comfortable and familiar with the VeriSafe AVT. Often they will realize how simple and efficient it is and it makes their job a lot quicker and easier. The key benefit is safety where you do not need to open the door to perform your absence of voltage test and the green LED gives you the assurance and reduces all of your hazards before you even open the door.
Another way is have customers form a safety group that includes every department (operators, electricians, engineers, etc.). When you are doing safety analysis at your plant floor, this safety group will give total buy-in for your safety program and the employees will be more open to try new ideas.
Q4: Could you please give us a manual or procedure for AVT installation? Answer: You can go to
www.panduit.com/VeriSafe where the installation manual and the connection options document are on the landing page. The connection options document visually shows you different ways on how to install the VeriSafe Sensor Leads, and includes best practices which will aid you in the installation procedures.
Q5: Does Panduit have any plans to come out with VeriSafe that can be applied for higher voltages, the medium or the HV? Answer: Yes, we are currently working on a VeriSafe that will go up to 1000 volts for DC applications. We also have a VeriSafe for medium voltage up to 13.2 KV in our product roadmap. This is still in the development stage and we are unable to give the exact timeline on when it will be available. We assure that the new version will also meet the rigorous safety standards as the first version of VeriSafe.
Q6: How many connecting cables / accessories would be required for establishing communication which comes under “System Cable” component. Answer: The system cable connects the Isolation module to the Indicator module. Only two connections are required.
Q7: Please share the list of customers who are already using VeriSafe at their Motor control centers.
Answer: We have active engagement with Rockwell, ABB/GE, EATON and Schneider.
Q8: What is the minimum voltage that the AVT will detect, as maximum is 600V? Answer: The VeriSafe AVT will detect voltage from 3-600V.
Q9: If two leads per phase are allowed for installation, can you suggest how many leads to be procured and what will be the total cost post installation of AVT? Answer: The sensor leads (2 per phase) are hardwired to the device and included with the VeriSafe. Total cost depends on the connection type used (see
connection options document for further details).