As a leading provider of Balance of System (BOS) components for the Solar industry, our robust physical infrastructure solutions have evolved to play a vital role in renewable energy production facilities worldwide. Panduit’s broad portfolio offers 75% of a BOS, which covers more ground than any other manufacturer. Combine this with direct access to expert consultants and strategic R&D investments that maximize efficiencies and decrease the total cost of ownership across the entire project.
As the solar industry has grown, Panduit’s physical infrastructure expertise has evolved to play a vital role in renewable energy production facilities around the globe. Over the last decade, Panduit has been leading the way, partnering with EPCs and solar installers on PV installations totaling more than 5GW of capacity.
Our combination of engineering and manufacturing expertise means our full portfolio of solutions is broad and deep, covering up to 75% of a typical photovoltaic (PV) installation electrical BOS. You won’t find another supplier that can provide this level of expertise. With infrastructure more crucial to cost savings than ever, it’s the approach you need.
Whether you need to ground, route, connect, protect, or identify your solar energy infrastructure, we have reliable power from the ground up providing efficiency and cost savings for large and utility-scale PV projects.
A typical PV system is composed of one or more solar panels combined with an inverter and other electrical and mechanical hardware that use energy from the sun to generate electricity.
Partner with us today to see how Panduit solutions can play a role in your infrastructure.
80 MW Arlington, GA
492 MW McCamey, TX
120MW Arlington, AZ
250MW Otay Mesa, CA
Mortenson Buildings Batter Energy Storage
754MW Cohuila, Mexico
19MW Turebylille, Denmark
102MW Hyogo, Japan